A factory reset will reset your console server back to its original factory default settings. The IP address will reset to 192.168.0.1.
There are three ways to reset the console server to factory defaults:
- Use the Web console.
- Use the Erase button.
- Use the command line.
Use the Web Console
Check both Config Erase and Reboot in the System → Administration menu and then click Apply.

Use the Erase Button
Use a ball-point pen to depress the recessed Erase button:
- Depress the Erase button twice within a 2 second period.
- Depress the button while the unit is powered ON.
- Depress the button gently.
Use the Command Line
To perform a factory reset from the command line, type
flatfsd -i