USB Charging and Power Delivery
Originally designed as a data interface with only limited power delivery capabilities, Universal Serial Bus (USB) has become a primary method of powering and charging mobile devices. In this article, we cover the capabilities of the current crop of USB chargers.
There are four methods of distributing power between USB-enabled Hosts and Devices.
1 Default Power
The USB 2.0 specification allows Hosts to deliver 5V at 500 mA, for a total power output of 2.5 watts. USB 3.0 and 3.1 allow 5V at 900 mA (4.5W). Certified Hosts and Devices must limit their power delivery and consumption to these "default" power levels.
| Specifications | Max. Voltage | Max. Current | Max. Power |
|---|---|---|---|
| USB 2.0 | 5V | 500mA | 2.5W |
| USB 3.0 / USB3.1 | 5V | 900mA | 4.5W |
| USB Battery Charging (BC) 1.2 | 5V | 1.5A | 7.5W |
| USB-C Current Mode (non-PD) | 5V | 3A | 15W |
| USB-C / Power Delivery (PD)* | 48V | 5A | 240W |
* In 2021, USB-IF published the PD 3.1 specification, officially called Extended Power Range (EPR). At the same time, it updated the USB Type-C cable requirements to handle the higher voltage. If you want to charge or power devices such as a gaming laptop, e-bike or laser printer using PD 3.1, you must use a USB-C 2.1 cable.
2 USB Battery Charging Specification
The USB Battery Charging Specification allows devices to draw current in excess of the default power limits. The first version of the specification (BC 1.0) was released in 2007, followed by version 1.1 in 2009, and the current, BC 1.2, in 2010.
BC 1.2 introduced three types of downstream ports:
- Standard Downstream Port (SDP) - power is limited to the default power of the applicable USB specification (USB 2.0 or USB 3.x)
- Dedicated Charging Ports (DCP) - delivers power only (no data) up to 1.5A
- Charging Downstream Port (CDP) - capable of delivering both data and power up to 1.5A.
3 USB-C® Current Mode
USB-C ports without Power Delivery are capable of delivering 5V at 3A for a total of 15 watts. This is sufficient to charge a smartphone in about 30 minutes and a tablet in 2.5 hours.
4 Power Delivery Protocol
USB Power Delivery (USB-PD) refers to the protocol that allows a "power provider," a cable and a "power consumer" to agree on the current and voltage levels. Because power can flow in either direction, the role of provider and consumer can change at any time.
This smart charging protocol enables devices to negotiate voltage, current and direction of power and data flow over the USB cable. Negotiations are governed by power rules and offer a range of voltage and current configurations. For example, a phone needing 18W might negotiate 9V and 3A from the power source.
USB-PD is used by Apple® iPhone®, iPad®, MacBook Pro®, Google Pixel™, and other smartphones and portable devices.
Do All USB-C Cables Support PD?
Yes. All USB-C to USB-C cables have the Configuration Channel (CC) required to support PD communication, but don't necessarily support the full range of voltage/current levels specified by USB-PD. The current on a passive USB-C cable is limited to 3A so the most it can support is 3A x 20V = 60W. The length of a passive cable is also limited to 4 meters (13 ft). Cables that support Power Delivery greater than 3A are electronically marked and rated up to 100W (5A x 20V). Cables supporting Power Delivery 3.1 Extended Power Range (EPR) operation are rated up to 240W (5A x 48V).
Are special cables required for PD 3.1 Extended Power Range (EPR) operation?
USB-C to USB-C cables capable of Extended Power Range (EPR) have additional features so they can deliver the voltage and current range for USB Power Delivery EPR operation. The electrical components of EPR cables support 5A and voltages beyond the 48V required for EPR operation.
Can I use older USB-C cables with PD 3.1 devices?
Yes, older cables can still be used with PD 3.1 laptops and peripherals but at lower power levels. PD 3.1 cables are also backwards compatible with earlier standards so lower power devices like headphones can negotiate for the power they need.
Can I power my 4K display from my laptop instead of a wall outlet?
Yes, using a PD 3.1 capable USB-C cable, you can connect a large monitor to your laptop's PD 3.1 port, freeing up a wall outlet and eliminating an ugly power brick. And your laptop display will still work, giving you two screens to work with.
Do all USB-C ports have the same functionality?
No. Even though all USB-C ports look the same, the features they support can vary widely. For example, a USB-C port on a wall charger will only charge devices. Ports on laptops may vary in the level of power they supply and the speed of data transmission. Some laptop USB-C ports support data only, power only or a combination of the two so check your machine's specifications before buying peripherals.
What is Fast Role Swap?
The USB Power Delivery 2.0 specification includes Fast Role Swap (FRS), a feature that ensures connected devices can continue to function when power is interrupted. As the name implies, Fast Role Swap allows a provider of power (a Source) to quickly and automatically become a consumer of power (a Sink). For example, let's say a hub, acting as a Source, is providing power to a laptop and an external hard disk drive (HDD) when it is unexpectedly disconnected from the AC outlet. The hub signals to the other devices that it needs to swap roles and become a Sink. The laptop, detecting the Fast Swap signal from the hub, switches its role from Sink to Source and begins supplying power from its battery to the hub and (indirectly) the HHD.
Other Fast Charging Standards
To make a device charge more quickly, most manufacturers will either increase the current (amps) or the voltage using one of the fast charging standards (e.g. USB-PD, Qualcomm Quick Charge™) or a proprietary fast charging protocol like Samsung® Adaptive Fast Charging or Motorola™ Rapid Charging.
Qualcomm Quick Charge™ (QC)
Chargers supporting the Qualcomm Quick Charge standard can quickly charge a range of devices. The current version, Quick Charge 5, will work with USB-A, USB-C and Micro USB cables but requires a USB-C cable for higher power 100W charging. QC5 is capable of charging a USB-C laptop in 2 hours.
In many ways, the QC standard is similar to USB-PD, particularly in its use of power negotiation protocols and variable voltage selection. But while Quick Charge is limited to phones and tablets that use Qualcomm's System on a Chip (SoC), USB-PD is more of an industry standard adopted by a wide swath of the market, including laptops.
What's Next for USB Charging?
As more devices integrate USB Type-C® ports for data transfer, expect to see manufacturers to take advantage of its power and Alt Mode capabilities too. For example, Apple's MacBook Air® ships with a 30W USB-C Power Adapter. Google's Pixelbook has a USB-C port on either side so you can charge and connect to an external monitor at the same time.
Currently, USB is still a confusing maze of specifications, data transfer rates, wattages and video resolutions. But as USB-C, PD 3.0 and USB4 converge in a new crop of laptops and peripherals due early 2021, a single port world may be just around the corner.
New GaN chargers like this one are smaller and charge everything from phones to laptops
If I have a GaN charger, can I leave my laptop AC adapter at home?
You absolutely can. If your laptop has a USB-C port, you can use your GaN wall charger to power and recharge the laptop and leave the bulky AC adapter at home. Small, lightweight GaN wall chargers can also provide power for your phone and tablet.
Products Mentioned in this Article
Why Buy from Eaton?
We know you have many brands to choose from. On the surface, they may all seem alike. It's what you don't see that makes the difference. With Eaton, you get solid engineering, proven reliability and exceptional customer service. All our products undergo rigorous quality control before they are offered for sale, and independent testing agencies verify our products meet or exceed the latest safety and performance standards. Our commitment to quality allows us to back our products with industry-leading warranties and responsive customer service. It's the Eaton difference.