What Type of UPS Do I Need?

January 20, 2022 Tripp Lite
what are the types of uninterruptible power supplies

An uninterruptible power supply, also known as a UPS system, protects connected equipment from power problems and provides battery backup power during outages. Some UPS systems also regulate abnormal voltages.

UPS systems protect against downtime, damage and data loss.

Downtime: Blackouts and brownouts (low voltage) shut down equipment. UPS systems supply battery backup power to support equipment through blackouts. Select models feature automatic voltage regulation (AVR) to correct incoming power without relying on UPS batteries.

Damage: Surges and line noise can damage internal components in a single devastating event or slowly over time. UPS systems feature surge protection and line noise filtering to guard equipment against potential damage.

Data Loss: When power problems shut down equipment, valuable data is often lost. UPS systems feature battery backup power to allow enough time for data to be saved.

Buying a UPS for your desktop, network or server rack involves a number of considerations, such as price and power capacity. Before delving into the details, first determine the type of UPS you need.

UPS Types

There are three main types of UPS battery backup, categorized by how they work: standby, line-interactive and on-line. Standby models provide a basic level of protection from power problems. Line-interactive models provide a higher level of protection than standby models, and on-line models provide the highest level of protection available.

Let’s take a look at each type individually.

Standby

Standby UPS systems have three main components: a surge/noise filter, a battery and an inverter/charger. During operation under normal voltage conditions, the UPS passes input voltage through the surge/noise filter before delivering it to connected equipment. It also uses its inverter/charger to charge the battery, preparing it for use during a blackout or brownout. During operation under blackout conditions, the UPS converts DC power from the battery into AC power to support connected equipment.

standby-operation

Standby UPS systems are very effective at what they are designed to do: provide a basic level of protection and support for connected equipment. Unlike line-interactive UPS systems, they rely on their battery to correct overvoltages and undervoltages. In areas that experience frequent voltage fluctuations, users should consider purchasing a line-interactive UPS instead of a standby UPS.

Line-Interactive

Every line-interactive UPS system includes a voltage regulator. By using its voltage regulator to adjust abnormally high or low voltage, line-interactive UPS systems reduce reliance on the battery, lengthening its service life. During operation under normal voltage conditions, the UPS passes input voltage through the surge/noise filter and the voltage regulator before delivering it to connected equipment. It also uses its inverter/charger to charge the battery, preparing it for use during a blackout or brownout. During operation under blackout conditions, the UPS converts DC power from the battery into AC power to support connected equipment.

line-interactive-operation

Line-interactive UPS systems provide an effective means of protecting equipment against power problems. Unlike on-line models, however, line-interactive UPS systems do not remove harmonic distortion.

On-Line

On-line UPS systems work very differently than line-interactive. During normal operation, on-line UPS systems continuously “remake” input power in a two-step process: first, converting AC power into DC power, then converting DC power back into AC power with a pure sine wave. This two-step process allows on-line UPS systems to supply connected equipment with the best quality output power available. Constant double-conversion on-line operation completely isolates sensitive equipment from every problem on the AC power line. During operation under blackout conditions, the UPS converts DC power from the battery into AC power to support connected equipment.

on-line-operation

In addition to categorizing UPS systems by how they work, they can also be further subdivided.

Output Capacity: UPS systems can be ranked by the maximum amount of power (expressed in both VA and watts) that equipment is able to draw from the UPS’s outlets or hardwire output terminals. “VA” stands for “volt-amps.” The VA of a device can be determined by multiplying its operating voltage by its amperage rating. For example, a 120V, 2.5-amp device would draw 300VA from a UPS’s output (120 x 2.5 = 300).

Configuration: UPS systems can also be subdivided by the types of cabinets they are housed in—rack-mount, tower, low-profile, undermonitor, etc.

Intelligent Operation: Within the line-interactive category, there are two subcategories—those that feature intelligent operation and those that do not. UPS systems that feature intelligent operation include a microprocessor that allows the UPS to relay more detailed operating conditions through power management software. All on-line UPS systems feature intelligent operation.

Extended Run Capability: Within the line-interactive and on-line categories, there are two subcategories—those that accept connection of additional internal or external batteries and those that do not. Those that accept additional batteries allow users to extend battery backup runtime for critical systems during a blackout.

Take a look at this chart for a side-by-side comparison:

  Standby Line-Interactive On-Line
  Standby Line-Interactive On-Line
TYPICAL USE Desktop computers, home networks Desktop computers, network workstations, network server racks, office networks Mission-critical equipment in data centers and server rooms
Battery Backup
Emergency backup power for utility power outages
YES YES YES
Surge Protection
Protection against power surges or spikes
YES YES YES
Brownout Protection
Maintains safe voltage levels without using battery power
NO YES YES
Overvoltage Protection
Keeps overvoltages from damaging connected equipment without using battery power
NO SOME YES
Pure Sine Wave Output
Perfect power for sensitive electronics
SOME SOME YES
Fully Online Operation
Zero transfer time to battery
NO NO YES

If you only need a basic level of protection—for low-power devices like desktop computers, gaming consoles or wireless routers—a standby model should suffice. For higher-power devices, a line-interactive or on-line model would be your best bet. Both offer network-grade protection, but neither is as cost-effective as a standby model.

Line-Interactive vs. On-Line UPS Systems

line-interactive-vs-on-line-performance
Transfer Time

Which performs better during a blackout: an on-line UPS or a line-interactive UPS? Line-interactive UPS systems provide a slight delay—around 4 milliseconds—during the transfer between utility and battery power. While the vast majority of equipment can tolerate such a transfer and both types perform well, on-line UPS systems set the highest standard.

On-line UPS systems provide a smoother transfer between utility and battery backup power. Because their batteries are integrated into their normal operation, on-line UPS systems take no time at all to transfer between utility and battery power—zero milliseconds. Zero transfer time allows on-line UPS systems to reliably support even the most sensitive devices. If an on-line UPS experiences an internal fault or overload, it will automatically “bypass” its internal components and deliver power directly to connected equipment. Additionally, on-line UPS systems feature an external bypass switch that allows users to perform the same function manually for scheduled maintenance.

Output Voltage Regulation

Which UPS provides the best output quality when regulating voltage—an on-line UPS or a line-interactive UPS? Line-interactive models regulate voltage within 12% ± of nominal voltage, while on-line models regulate within 2%. While the vast majority of equipment can tolerate such a voltage range and both types perform well, on-line UPS systems set the highest standard.

Maintenance

What if the UPS requires maintenance, but the connected equipment cannot be turned off and must continue to receive power? While on-line UPS systems can be safely maintained while still providing continuous power to connected equipment, most line-interactive UPS systems cannot. The difference is in the on-line UPS system’s power bypass features.

bypass-switch

If an on-line UPS system experiences an internal fault or overload, it will automatically “bypass” its internal components and deliver power directly to connected equipment. In addition, on-line UPS systems feature an external bypass switch that allows users to perform the same function manually. While select Tripp Lite line-interactive UPS systems feature an automatic internal bypass function, none feature a manual external bypass switch.

    ABOUT TRIPP LITE BY EATON

    Tripp Lite joined the Eaton family in March 2021. Eaton has long been a premier name in backup power and power management. The acquisition of Tripp Lite transforms Eaton’s distributed IT infrastructure and connectivity equipment capabilities. Combining our product strengths and expert personnel allows us to offer comprehensive and innovative solutions for critical power and digital infrastructure applications, backed by quality, service and support you can trust. Learn more at tripplite.eaton.com/byEaton.

    Subscribe to This Blog

    Recent Posts

    Have a Question?