Cat6 vs Cat6a Ethernet Cables – Everything You Need to Know

Cat6 has become the go-to cable standard for network installers. If you’re wondering whether you should use standard Cat6 or the more robust Cat6a, keep reading.

You can think of Ethernet cables as the plumbing system of your network. If your house has rusty or clogged pipes, you’ll probably have contaminated, low-pressure water coming out of your faucets. Similarly, if you use older Ethernet cables, such as Cat5 or Cat5e cables, you’re more likely to experience slow network speeds and signal interference. Basically, higher quality Ethernet cables can improve network performance.

Just like most other forms of technology, Ethernet cables have dramatically improved in functionality over the past decade. Currently, it’s considered a best practice for businesses to use Cat6a, replacing the Cat6 cables that used to be considered the gold standard. Speed and distance capabilities are several of the reasons why Cat6a has rapidly outpaced standard Cat6.

Cat6 versus Cat6a

The “a” in Cat6a stands for augmented. The chart below shows some of the major differences between the two types of cable:

Cat6Cat6a
FrequencyUp to 250 MHzUp to 500 MHz
Maximum Cable Length328 ft./100 m for slower network speeds
(under 1 Gbps);
180 ft./55 m for Gigabit Ethernet
328 ft./100 m, regardless of network speed
Hypothetical Top Speed10 Gbps (over 110-180 ft./33-55 m)10 Gbps (over 328 ft./100 m)
ConnectorsRJ45RJ45

As the above chart illustrates, Cat6a cables support high-speed data transfer over longer distances than Cat6 cables. Cat6a cables are also a future-proof solution that can handle network upgrades.

Cat6a cables were around 50% larger than Cat6 cables when they were first introduced, but the size of the cables has been reduced by around 10% in recent years. Much of the extra size (and weight) is due to the superior shielding on Cat6a cables, which reduces interference.

Compatibility

If you are considering installing Cat6 or Cat6a cables in an older network, both are compatible with 10BASE-T and 100BASE-T standards. Cat6a cables are typically more cost-effective because they will not need to be replaced during network upgrades.

Upgrading from Cat6 to Cat6a is easy because both cables use RJ45 connectors.

Choosing the Right Cable

Tripp Lite offers hundreds of Cat6 and Cat6a cable solutions. Contact our team of Chicago-based product experts for guidance when evaluating the cable in your network.   

Browse Cables

Contact Us

Which Ethernet Cable Should You Use — Cat5e, Cat6 or Cat6a?

The decision of whether to use Category 5e, 6 or 6a cables to wire your Ethernet network pretty much comes down to cost, data transfer speed and connection distance. All use RJ45 connectors to patch into your network via server, router, computer or other hardware. As well, all support Power over Ethernet (PoE). Otherwise, each cable has a different standard. [Read more…]