Which Type of UPS System Works Best with a Generator?

Do you have a generator to supply power during a lengthy blackout? You’ll get the most out of it if you connect your generator to a UPS system. But there’s more than one kind of UPS – it’s important to choose the right type of system so it will play nicely with your generator power. [Read more…]

Pure Sine Wave vs. Modified Sine Wave

In regard to output waveform, two types of UPS systems exist—the kind that produce a pure sine wave and the kind that produce a stepped approximation of a sine wave, also known as a pulse-width modulated (PWM) sine wave. The main difference between pure sine wave and modified sine wave systems is that a pure sine wave system in battery backup mode is guaranteed to produce a cleaner output for any piece of equipment connected to it, whether it’s a computer at a workstation or a server in a data center. The same cannot be said of a modified system, which produces a step, or PWM, sine wave output. Its output is choppier and provides equipment with a less stable output waveform.
[Read more…]

Keep Your IP Camera Installation Up and Running Through Power Problems

Security Camera

For home and small business owners, installing a video surveillance system is one of the most effective ways to protect assets and deter theft. But after your system is up and running, you’ll want to ensure that it stays that way. An uninterruptible power supply, or UPS system, will keep your cameras going in the event of a power surge or outage.

[Read more…]

Centralized vs. Decentralized UPS Systems

One of the first steps in choosing the most appropriate UPS solution is deciding whether to use a centralized or decentralized setup. While both have their advantages, knowing how to answer this question depends on a number of factors.

Here are five things to consider when deciding between a centralized and decentralized solution: [Read more…]

Protect Your Fish, Plants and Equipment with UPS Battery Backup for Aquariums

One never knows when a power outage may strike, and if you own fish and other sea creatures, you should be prepared with an uninterruptible power supply (UPS) for your aquarium. Heaters, aerators, filtration systems—all need electrical power to operate and keep fish alive. They need heat when it is cold, cold when it is hot, and oxygen to breathe at all times.

An aquarium battery backup system can prepare you for the next unexpected power outage. By purchasing a UPS system for your fish tank, you can ensure that your essential equipment will continue providing life-giving power.

Before choosing a UPS system, you’ll need to measure your total load. That is, the total number of watts put out by your life-sustaining equipment such as filters, aerators and heaters. Be sure your aquarium battery backup system can handle more watts than the total load of your equipment. Also, you may want to consider the amount of runtime you’ll need, in case the outage is longer than anticipated. Most power outages last from just a few minutes to less than an hour. If you still need help calculating the capacity (load) of your aquarium and determining the desired battery backup runtime, checkout this UPS sizing guide.

One more point to consider: pure sine wave power. Many popular brands of electric motors for aquarium filters and aerators require pure sine wave power to operate. Incorrect power output can result in motors running slowly, erratically, or not at all when the UPS is on battery. Thus, you’ll need a fish tank UPS that generates pure sine wave power, as the following choices do.

[Read more…]