What’s the Difference Between Surge Protectors, Line Conditioners and UPS Systems?

Your options for protecting home and office electronics from power problems can be a bit confusing. Surge protectors, line conditioners and uninterruptible power supplies (UPS systems) all have outlets for AC equipment, protect against power surges and filter line noise to help prevent EMI/RFI interference. Line conditioners and UPS systems, however, have additional types of protection. Your best choice for power protection depends on your equipment, your application and the quality of your facility’s electricity.

Surge Protectors

Reliable Surge Protection and Line Noise Filtering

Surge protectors are your best defense against AC voltage surges and spikes that can ruin your valuable equipment in a flash or build up damage over time. Look at the joule rating when comparing surge protectors – a higher rating means more protection. Some models even protect phone and data lines. Surge protectors also help prevent EMI/RFI line noise from interfering with equipment performance.

Line Conditioners

Voltage Regulation, Surge Protection and Line Noise Filtering

Line conditioners are your best defense against brownouts, which are low-voltage power sags that can cause your equipment’s internal power supply and circuitry to work harder. Frequent exposure to brownouts can overheat these sensitive components, leading to equipment failure. Line conditioners automatically adjust low and high voltages to provide safe computer-grade power. In addition to voltage regulation, line conditioners offer surge protection and line noise filtering.

UPS Systems

Voltage Regulation (Line-Interactive and On-Line Models), Battery Backup, Surge Protection and Line Noise Filtering

UPS systems are your best defense against downtime, damage and data loss. All UPS systems provide battery backup to keep equipment up and running through short blackouts and brownouts, providing you with enough time to save data and shut down properly during longer outages. A UPS system can also keep equipment powered during transfer to generator power.

There are three types of UPS systems, each with different features:

  • Standby: Provide battery backup, surge protection and line noise filtering.
  • Line-Interactive: Provide voltage regulation, battery backup, surge protection and line noise filtering.
  • On-Line: Provide the highest level of power protection. Constant on-line operation completely isolates sensitive equipment from every power problem on the AC line.

Communication ports are also a useful feature to have on UPS systems. Most Tripp Lite standby UPS systems and all line-interactive and on-line models are compatible with Tripp Lite’s free PowerAlert software, which can automatically and gracefully shut down computers during a prolonged power outage.

Feature Comparison

 
Surge
Protectors
Line
Conditioners
Standby
UPS Systems
Line-Interactive
& On-Line
UPS Systems
Surge Protection
Brownout Protection
EMI/RFI Line Noise Filtering
Voltage Regulation
Battery Backup
Typical Connected Equipment Computers and Peripherals, Home Theater Electronics Computers, Laser Printers, Industrial Equipment, Refrigerators, Air Conditioners Desktop Computers and Peripherals Servers/Network Equipment
  VIEW PRODUCTS VIEW PRODUCTS VIEW PRODUCTS VIEW PRODUCTS

Need help choosing power protection for your equipment?

Contact a Tripp Lite Power Specialist. Our advice is always fact-based and free.

What Are Surge Protector Joules and How Many Do I Need?

Among the factors to consider when choosing a surge protector – how many outlets, the optimal cord length and options such as protection for a coaxial cable connection – perhaps the most important factor is the surge protector’s joule rating. [Read more…]

Will Your Surge Protector Still Protect Your Equipment After a Power Surge?

Isobar-Group-(4-6-8-outlets)-view-dynamicLet’s say you had a weather-related power surge at your home or facility, and you had all your important electronic equipment protected by a surge protector. Your connected equipment is working properly post-surge, so you assume the surge protector did its job. But now you’re wondering, “What about next time?” How do you know if the previous power surge damaged your surge protector to the point where it will no longer provide the same level of protection? The answer depends on the severity of the power surge and what type of surge protector you have. [Read more…]

How To Select a Surge Protector for a Home Theater System

HT10DBS-FRONT-LInvesting in a surge protector that’s designed for home theater equipment is a small price to pay in order to protect your very expensive equipment from the unforeseen consequences of power surges or electrical line noise. But selecting a surge protector can be a daunting task. To make the job easier, here is a checklist of things to consider when selecting a surge protector for a home theater system.

 

 

Type of Equipment: What kind of equipment will you be plugging into your surge protector? Home electronics, computers, office equipment and workbench tools have different protection needs. Be sure to choose a surge protector that protects your equipment on all inputs, including telephone lines (RJ-11), computer network (RJ-45) and cable jacks (coaxial).

Cord Length & Plug Design: Determine how far you will place your surge protector from your grounded AC outlet, and select a surge protector with a cord at least that long. If you want to place furniture flush against the wall in front of the AC outlet, choose a surge suppressor with a right-angle plug.

Number of Outlets: Determine how many items you will be plugging into your surge suppressor, and purchase one with at least as many outlets as you expect to need. Remember that transformer plugs are wider than standard plugs. Select a surge protector that will accommodate transformer plugs without blocking adjacent outlets.

Indicator Lights: Most surge protectors include diagnostic LEDs that confirm power availability and protection status. After repeated power surges, the protective circuitry will burn out so it’s important to know whether or not your surge protection is still functioning.

Protection Modes: Residential power outlets have three wires: hot line (H), neutral (N), and ground (G). Since your home theater equipment is connected to all three, you need a surge protector that protects all three lines, covering the two protection modes: full normal mode (H-N) and common mode (N-G / H-G).

Safety Testing: Underwriters Laboratories (UL) is facility that conducts independent, product safety testing. Surge suppressor manufacturers use UL to test their products according to the UL 1449 safety testing standard. There are several editions to the UL 1449 testing standard. The most current one is the 3rd Edition, which tests to a higher degree of safety than earlier editions. The best surge protectors for home theater equipment conform to the UL 1449 3rd Edition.

_________________________________________________________________________________________________________________________________________________________________

Those are the easy things to consider when selecting a surge protector for a home theater system. The more difficult things cover the protection level ratings. By understanding and interpreting their meaning, you will be able to select the most appropriate surge proctor for your home theater system:

Response Time: The response time tells you how long it takes for the surge suppressor to turn on before it is actively preventing a surge from affecting your equipment. The response time is rated in nanoseconds (billionths of a second). The lower the number, the faster the response. The best surge protectors for home theater equipment have less than a one nanosecond response time.

Clamping Voltage: While the response time tells you how quickly a surge suppressor takes to “turn on,” the clamping voltage tells you at what level of surge voltage the suppressor turns on. High clamping voltages allow a higher level of surge voltage to get to your equipment. So, the lower the clamping voltage rating, the better the protection. The best surge protectors for home theater equipment have clamping voltages of 140V.

Energy Absorption: A surge or spike in its most basic terms is raw electrical energy. And energy cannot simply disappear, it has to be either dissipated as heat or absorbed by something else. Surge protectors absorb surge energy and divert it away from your sensitive home theater equipment. Therefore, its energy absorption capability, rated in joules, is a good indicator of the quality of the surge protector. The higher the joule rating, the better the energy absorption. The best surge suppressors for home theater equipment have a joule rating over 3000.

EMI/RFI Filtering: Electromagnetic interference (EMI) and radio frequency interference (RFI) cause data loss, A/V interference, and sometimes even computer memory loss. The EMI/RFI filtering is rated in decibels (dB). The higher the number, the better the protection. The best noise filters for home theater equipment have about a 60dB rating.

Maximum Surge Amps: This represents the maximum current that the suppressor can tolerate before the surge damages the suppressor itself. The higher the number, the better the surge suppressor. The best surge suppressors for home theater equipment have ratings as high as 150,000 amps.

Finally, there are a few other considerations you should address while shopping for a surge protector. Some surge protectors come with a warranty that covers the replacement of your computer and audio/visual components if the surge protector fails. Another consideration would be a surge protector’s energy efficiency. If energy efficiency is important to you look for a “green” surge protector, which has special circuitry to reduce energy consumption.

Get More Information on Surge Protectors for A/V and Home Theater Equipment

The Importance of Power Protection for Office Workstations

Everyone recognizes the importance of backing up the data center, but overlooking the workstation is an all-too-common mistake. Office workers’ productivity depends on the smooth operation of their desktop workstations. [Read more…]