Which Type of UPS System Works Best with a Generator?

Do you have a generator to supply power during a lengthy blackout? You’ll get the most out of it if you connect your generator to a UPS system. But there’s more than one kind of UPS – it’s important to choose the right type of system so it will play nicely with your generator power. [Read more…]

Connect Your Laptop to the Internet without a Built-in Ethernet Port

Laptop computers are trending toward thinner models that do not include an Ethernet port. If you rely on Wi-Fi day-to-day, you may not notice the change. But in situations where Wi-Fi is weak or unavailable, you can count on a USB 3.0, 3.1 or USB-C to Gigabit Ethernet Adapter to get the signal you need.

No ethernet in laptops

The Lighter Laptop

As laptop users run more browser-based applications and store more files in the cloud, they require less local storage space. This, combined with smaller and more efficient processors, means laptops can afford to be thinner and lighter without sacrificing performance.

When laptop manufacturers shrink their products to facilitate more portability, some connectivity features may not “make the cut.” These often include the Ethernet port since it is, quite literally, thicker than the device.

Again, even if you typically use a wireless internet connection, consider some scenarios where an Ethernet connection might be missed:

[Read more…]

Rolling TV Carts for Education

Use Rolling TV Stands to Help Enhance Learning on a Tight Budget

dmcs60100xx

Do more with less. This is the challenge facing virtually every school, particularly when it comes to in-classroom technology.

Not everyone learns the same way, but strong visuals enhance learning for most students. That’s why TVs and interactive white boards are common tools for today’s teachers. However, keeping classrooms equipped with the latest technology might quickly break the budget.

Cut Costs with Shared Resources

With a rolling TV cart for flat-screen TVs, a school can keep technology expenditures in check by sharing displays and interactive white boards among a number of classrooms. When the lesson plan calls for A/V resources, the teacher simply wheels a height-adjustable TV stand in front of students to make learning more engaging and exciting. And by using the built-in adjustments such as height and tilt that are found on many rolling TV stands, the teacher can ensure all students have a clear view of the screen. This isn’t possible with conventional projectors.

[Read more…]

Pure Sine Wave vs. Modified Sine Wave

In regard to output waveform, two types of UPS systems exist—the kind that produce a pure sine wave and the kind that produce a stepped approximation of a sine wave, also known as a pulse-width modulated (PWM) sine wave. The main difference between pure sine wave and modified sine wave systems is that a pure sine wave system in battery backup mode is guaranteed to produce a cleaner output for any piece of equipment connected to it, whether it’s a computer at a workstation or a server in a data center. The same cannot be said of a modified system, which produces a step, or PWM, sine wave output. Its output is choppier and provides equipment with a less stable output waveform.
[Read more…]

Where There’s Power, There’s a Power Cord

Even in today’s increasingly wireless world, most IT equipment requires an AC power cord.

When you installed your servers, routers or other devices, you connected the power cables and probably haven’t thought about those cords since. But there are several good reasons to consider replacing or upgrading the power cords on your equipment. [Read more…]