Use Hospital-Grade Power Cords for Safe Connections in Healthcare Settings

Hosptial-Grade Power Cord

Hosptial-Grade Power Cord

Hospitals, clinics and other medical offices must adhere to safety regulations defined by the National Fire Protection Association’s Life Safety Code to ensure safe, reliable power and help protect patients and staff from shocks and other hazards.

The code includes requirements regarding the use of power cords. To be rated as hospital-grade for use in healthcare environments, power cords undergo rigorous testing to ensure they meet stringent UL standards, specifically UL 817 and CAN/CSA C22.2 no. 21 for use outside of the patient-care vicinity.

At the heart of UL’s standards for hospital-grade power cord sets are requirements for the plug. The blades must be solid, instead of folded brass. The plug must include an internal cable retention device or flexible strain relief to prevent stress to the plug’s internal connections. The plug will be marked “Hospital Grade” and have a visible green dot.

[Read more…]

The Importance of Smart PDUs in Cryptocurrency Mining

Bitcoin and Beyond

bitcoin
Bitcoin is the world’s first cryptocurrency, described by its inventor, Satoshi Nakamoto, as “a new electronic cash system that uses a peer-to-peer network to prevent double-spending…completely decentralized with no server or central authority.” Since Bitcoin’s 2009 debut, more than 900 cryptocurrencies have flourished, including the popular Ethereum and Litecoin.

Cryptocurrencies can survive only due to miners, who confirm every transaction and add it to a blockchain. Miners are then rewarded with Bitcoins or other cryptocurrencies, but it can be difficult to keep up with the expenses involved in a successful mining operation. As you know, one must bring in more Bitcoins than one spends to be profitable!

[Read more…]

The Benefits of Antimicrobial Power Strips for Healthcare Facilities

Tripp Lite Antimicrobial power strip outlet view

The Centers for Disease Control and Prevention estimate nearly two million hospital patients in the U.S. annually contract a healthcare-acquired infection (HAI), at a cost over $36 million a year.

Frequently, HAIs are spread through cross-contamination when objects are handled by multiple people. Any object in a healthcare setting touched by staff, patients or visitors becomes a potential breeding ground for harmful microbes such as C. diff and MRSA. The threat of HAIs is especially significant within the patient-care vicinity, where patients receive their treatments.

Hidden Sources of HAIs

Think of frequently handled objects in a hospital and what likely comes to mind are door handles, light switches and elevator buttons. Not so obvious are objects used in the treatment of patients that may need to be moved from one room to another, thus increasing the chances of transferring bacteria and viruses. Medical facilities often use carts holding equipment that needs to be plugged in. The assembly on the cart may include a special-purpose relocatable power strip, also known as a power strip.
[Read more…]

Keep Your IP Camera Installation Up and Running Through Power Problems

Security Camera

For home and small business owners, installing a video surveillance system is one of the most effective ways to protect assets and deter theft. But after your system is up and running, you’ll want to ensure that it stays that way. An uninterruptible power supply, or UPS system, will keep your cameras going in the event of a power surge or outage.

[Read more…]

Where There’s Power, There’s a Power Cord

Even in today’s increasingly wireless world, most IT equipment requires an AC power cord.

When you installed your servers, routers or other devices, you connected the power cables and probably haven’t thought about those cords since. But there are several good reasons to consider replacing or upgrading the power cords on your equipment. [Read more…]