Tripp Lite by Eaton Blog

Charging and Securing Tablets in Healthcare Facilities

Written by Tripp Lite | Apr 4, 2016 5:00:00 AM

The increased use of tablets in medical facilities has revolutionized healthcare services, from on‑the‑go chart documentation to patient intake, registration and point-of-service surveys.

Tablets make medical information more robust and accessible for healthcare workers in all settings, but the technology presents a host of challenges, too: how do office managers and administrators ensure tablets are kept charged for use, stored securely and updated when necessary? Tripp Lite’s Charging Stations are the perfect solution.

For iPad and Android tablets, USB Charging Stations provide 2.4 amps of USB charging for up to 16, 32 or 48 devices. For Chromebooks, notebook computers and laptops, AC Charging Stations accommodate up to 16 or 32 computers with 1,440 total watts of charging power.

The Charging Stations can be mounted to a wall, countertop or table, or used as a mobile cart, making them ideal for all healthcare environments. When used as a cart, devices can be deployed easily to physicians, nurses and technicians who may work in different departments or on several floors.

To help healthcare facilities comply with medical information privacy regulations, the Charging Stations have locking doors and side panels to prevent unauthorized access and protect the devices from theft. All sides of the cabinets are constructed from sturdy steel with a powder-coated finish for long-term durability. Flow-through ventilation prevents overheating, even while several devices charge simultaneously.

As if that weren’t enough, these Charging Stations also feature removable dividers for flexible configurations within the cabinet. The shelves are coated to shield devices from scratches and scuffs, and solid tops on select models can double as a handy work surface.

Browse the full line of Tripp Lite Charging Stations